Either MFRC522 or PN532 is compliant with ISO14443-4 Type Tag?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Either MFRC522 or PN532 is compliant with ISO14443-4 Type Tag?

5,414 Views
gokhan_tasci
Contributor I

Hi,

I'm trying to read ISO14443-4 type NFC Tag with MFRC522 or PN532 based NFC reader board. Are these ICs  compliant with ISO14443-4?

Tag's info which is scanned with NXP's Tag Info App from Google Play store is Attached.

Best regards.

0 Kudos
Reply
1 Reply

4,870 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear Gökhan Taşçı,

both readers support MIFARE and iso 14443 so there should not be any problem interacting with layer 4 tags the thing here is that you might have to implement some commands for that layer since both of those products are no longer recommended for new designs,  please check their replacement for :

MFRC52202HN1  - > MFRC630 | High-performance MIFARE and NTAG Frontend for Access | NXP  

PN532  -> PN7150 | High performance NFC controller for smart devices | NXP 

the image you attach is not from tag info is from NFC tools. but it should be supported by 

BR

Jonathan

0 Kudos
Reply