Trouble finding RFIDdiscover full version on docstore

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trouble finding RFIDdiscover full version on docstore

359,851 Views
novo
Contributor I

I have trouble finding RFIDdicover full version on docstore.  Searching for “sw186641″ does not produce any results.

 

Also using RFIDdiscover Lite on Windows 10 fails to connect to Pegoda RD710.  Is there Windows 10 specific driver aside from the one that can be downloaded from NXP?

 

Thank you,

--Yuri

0 Kudos
Reply
2 Replies

359,846 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please search Sw186649 on DocStore. Please find it as the attachment. 

Hope it help you. Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply

359,371 Views
EmbExt
Contributor I

Search Results for  "Sw186649"

No results for "Sw186649"

Tags (1)
0 Kudos
Reply