Transfer data from PC to Android via NFC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Transfer data from PC to Android via NFC

1,865件の閲覧回数
alibigdeli
Contributor I

NFC   I  need to send some screen shots from my PC to my android device via NFC tags. How is that possible?

Thanks

タグ(1)
0 件の賞賛
返信
1 返信

1,636件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Bigdeli ,

The solution is possible, but not good, because RF transmitting speed is only 106Kbps. One of the 2 ways can be used :

(1) NFC reader is required on PC board.

(2) NFC reader module can be connected to PC USB

NFC reader IC can be NCP3000 or PN7150.

Actually, your solution can also use WIFI to transmit image data between PC & android device!

Regards,

Weidong

0 件の賞賛
返信