Transfer data from PC to Android via NFC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Transfer data from PC to Android via NFC

1,810 次查看
alibigdeli
Contributor I

NFC   I  need to send some screen shots from my PC to my android device via NFC tags. How is that possible?

Thanks

标记 (1)
0 项奖励
回复
1 回复

1,581 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Bigdeli ,

The solution is possible, but not good, because RF transmitting speed is only 106Kbps. One of the 2 ways can be used :

(1) NFC reader is required on PC board.

(2) NFC reader module can be connected to PC USB

NFC reader IC can be NCP3000 or PN7150.

Actually, your solution can also use WIFI to transmit image data between PC & android device!

Regards,

Weidong

0 项奖励
回复