Tamper alarm using G2iM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tamper alarm using G2iM

1,815 Views
Twsnhbb
Contributor I

Hello, 

We are attempting to use the tamper alarm feature with the G2iM+ IC. We are able to read and write the EPC on the tags as well as read the TID banks to identify the chips. However, when we attempt to access the alarm at either 0x200 or 0x20F we receive a PC OVERRUN error message and an exception is thrown. 

We are using a thingmagic M5e reader. Can anyone offer advice or support? We are also having the same issue accessing the memory address with our TSL 2128P reader. 

Thank you

0 Kudos
Reply
1 Reply

1,781 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi @Twsnhbb ,

first of all you have to make sure that you have a G2iM+ not a G2iM, the non plus version does not have the tamper alarm feature,  second, can you confirm that  you have checked the following appnote section 16.

https://www.nxp.com/docs/en/application-note/AN10940.pdf

BR

 

Jonathan

0 Kudos
Reply