SLRC61003 Schematics design question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SLRC61003 Schematics design question

2,041件の閲覧回数
bob_zhang
Contributor I

Customer is designing schematics using SLRC61003,there are two questions.

1 Their MCU power supply voltage is 2.5V,so they power VDD,PVDD and TVDD of SLRC61003 with 2.5V.I see the lower limit of these power is 2.5V in datasheet. Are there some potential risks for this design?

2 For TDO,TDI,TMS and TCK pins, If they don't use,how to deal with?Floating or Grounding?I find in demo design TDI,TMS and TCK are gounding  and TDO is floating.

I attach the schematic file,please help check.

0 件の賞賛
返信
1 返信

2,034件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Bob,

See below, please!

>>1 Their MCU power supply voltage is 2.5V,so they power VDD,PVDD and TVDD of SLRC61003 with 2.5V.I see the lower limit of these power is 2.5V in datasheet. Are there some potential risks for this design?

For SLRC61003HN, min voltage is no problem.

weidong_sun_0-1610446117561.png

In theory, there is no risk, but TVDD=2.5V, this voltage is relatively low, which will have an impact on the transmit power.

2 For TDO,TDI,TMS and TCK pins, If they don't use,how to deal with?Floating or Grounding?I find in demo design TDI,TMS and TCK are gounding and TDO is floating.

---You can design according to the method of DEMO board.

---In fact, there is no problem with these pins floating.

[Note]

  checked your schematic,  no other issues were found.

 Hope this information is helpful to you.

Have a nice day!

B.R,

Weidong

0 件の賞賛
返信