RF transmission speed selection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RF transmission speed selection

2,363 次查看
c_adharumaraj
Contributor I
Hi All,
We are using the PN553 NFC controller in an android device.
We want some information on how to select the RF speed used between the NFC card and the reader.
When we are reading type A/B NFC cards we observe that the RF transmission speed selected is 106kbps even though the card is capable of higher speeds.
When the card is used with third party readers we see the speed negotiated between the reader and the card is higher.
We tried modifying the NXP_CORE_CONF configuration in libnfc-nxp_RF.conf but there was no effect.
NXP_CORE_CONF={ 20, 02, 2E, 0E,
        28, 01, 02,
        ....

Can anyone please let us know if this is the right place to change? Else how can this speed can be configured?
0 项奖励
回复
2 回复数

2,218 次查看
trivedimanva
Contributor II

Hi Kan,

Can you please share & add more details on selecting speed using application and card end.

As I am using Mifare DesFire Ev1 8k card which supports RF speed with 106, 212, 424 & 848 kbps, but it unable to change speed accordingly.

Currently I have hard coded my values in "phpalI14443p4a_Sw_ActivateCard" function for specific speeds. From my point of view it is not a valid way to do it for changing speed for CL Type A L4 card ? please correct if it is wrong.

Kindly let us know that how does it actually works to get change the RF speed from card or application side.

Thanks 

Manva

0 项奖励
回复

2,338 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi ,

Usually the speed is changed automatically after a PPS request, so did your application issue this request to the card? 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复