PR5331 whether support to read 7816 type A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PR5331 whether support to read 7816 type A

2,237 次查看
michael_yang
Contributor II

we use NXP,PR5331C3HN/C370E NFC reader IC,  use 7816 type A card to read and will be USB disconnected. we don’t use this type of card 7816 type A before the test so no problem was found, we need to know PR5331 whether support to read 7816 type A or their software not add this drive?

标记 (1)
0 项奖励
回复
3 回复数

2,092 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please accept my apologies but this protocol is not supported by this device. For the supported protocols, please check chapter 1. General description of datasheet: https://www.nxp.com/docs/en/nxp/data-sheets/PR533.pdf 

Have a nice day!

BR,

Ivan. 

0 项奖励
回复

2,092 次查看
michael_yang
Contributor II

hello, 

NRR found that the usb communication link with PR533 is broken, if repeatedly calling the ISO/IEC14443 Type A command such as Select(AID) in each 2-3 seconds.

 

The following is the detailed scenario and PCSC log information of the problem. Please advise to fix the problem, thanks!

 

Scenario

  • Tested NRR (PCD) with mobile phone (PICC)
  • NFC-A mobile phone (PICC) with FWTI = 4
  • Continuously sending NFC-A commands as follows, and error occurs occasionally (usually within 15 min):

 

Normal Case

Error Case

(NRR)

REQA

REQA

(mobile)

ATQA

ATQA

(NRR)

ANTICOLLISION

ANTICOLLISION

(mobile)

UID CLn

UID CLn

(NRR)

SELECT

SELECT

(mobile)

SAK

SAK

(NRR)

RATS

RATS

(mobile)

ATS

ATS

(NRR)

APDU Command (e.g., Select AID)

APDU Command (e.g., Select AID)

(mobile)

(NRR)

…

S(WTX) Request

S(WTX) Response

S(WTX) Request

S(WTX) Response

…

S(WTX) Request

S(WTX) Response

S(WTX) Request

S(WTX) Response

S(WTX) Request

S(WTX) Response

…

S(WTX) Request

S(WTX) Response

(mobile)

APDU Response

S(WTX) Request

(NRR)

-

No response from PCD for ~1.5s

S(DESELECT) after 2s timeout

(mobile)

-

S(DESELECT)

  • Observation when error case happens:
    • No response from NRR
    • USB device (PR533) was found to be disconnected
    • Related PCSC log:

_[36m00000155_[0m _[35mifdwrapper.c:527:IFDTransmit() Card not transacted: 612_[0m

_[36m00000134_[0m _[35mwinscard.c:1606:SCardTransmit() Card not transacted: 0x80100016_[0m

_[36m00000127_[0m winscard.c:1626:SCardTransmit() UnrefReader() count was: 3

_[36m00000148_[0m winscard_svc.c:606:ContextThread() TRANSMIT rv=0x80100016 for client 9

_[36m00000618_[0m winscard_svc.c:317:ContextThread() Received command: DISCONNECT from client 9

_[36m00000264_[0m readerfactory.c:766:RFReaderInfoById() RefReader() count was: 2

_[36m00000164_[0m winscard.c:851:SCardDisconnect() Active Contexts: 8

_[36m00000132_[0m winscard.c:852:SCardDisconnect() dwDisposition: 0

_[36m00000153_[0m winscard.c:1044:SCardDisconnect() UnrefReader() count was: 3

_[36m00000167_[0m winscard_svc.c:488:ContextThread() DISCONNECT rv=0x0 for client 9

_[36m00000728_[0m winscard_svc.c:317:ContextThread() Received command: CONNECT from client 9

_[36m00000253_[0m winscard.c:235:SCardConnect() Attempting Connect to NXP PR533 (3.70) 00 00 using protocol: 0

_[36m00000158_[0m readerfactory.c:739:RFReaderInfo() RefReader() count was: 2

_[36m00000135_[0m winscard.c:422:SCardConnect() Direct access: no protocol selected

_[36m00000154_[0m winscard.c:429:SCardConnect() hCard Identity: 56653f3b

_[36m00000156_[0m winscard.c:490:SCardConnect() UnrefReader() count was: 3

_[36m00000167_[0m winscard_svc.c:451:ContextThread() CONNECT rv=0x0 for client 9

_[36m00010802_[0m winscard_svc.c:317:ContextThread() Received command: TRANSMIT from client 9

_[36m00000303_[0m readerfactory.c:766:RFReaderInfoById() RefReader() count was: 2

_[36m00000167_[0m winscard.c:1581:SCardTransmit() Send Protocol: T=4

_[36m00000219_[0m _[34mAPDU: FF C2 00 00 07 80 03 01 00 00 81 00 00 _[0m

_[36m00000145_[0m _[34mifdhandler.c:1262:IFDHTransmitToICC() usb:1fc9/010b:libudev:0:/dev/bus/usb/002/003 (lun: 0)_[0m

_[36m00001222_[0m _[01;31mccid_usb.c:660:WriteUSB() write failed (2/3): -99 Invalid argument_[0m

_[36m00000138_[0m _[34mSW: _[0m

_[36m00000146_[0m _[35mifdwrapper.c:527:IFDTransmit() Card not transacted: 612_[0m

_[36m00000130_[0m _[35mwinscard.c:1606:SCardTransmit() Card not transacted: 0x80100016_[0m

_[36m00000129_[0m winscard.c:1626:SCardTransmit() UnrefReader() count was: 3

_[36m00000357_[0m winscard_svc.c:606:ContextThread() TRANSMIT rv=0x80100016 for client 9

_[36m00000655_[0m winscard_svc.c:317:ContextThread() Received command: CONNECT from client 9

_[36m00000430_[0m winscard.c:235:SCardConnect() Attempting Connect to NXP PR533 (3.70) 00 00 using protocol: 0

_[36m00000156_[0m readerfactory.c:739:RFReaderInfo() RefReader() count was: 2

_[36m00000137_[0m winscard.c:422:SCardConnect() Direct access: no protocol selected

_[36m00000355_[0m winscard.c:429:SCardConnect() hCard Identity: 71b586eb

_[36m00000192_[0m winscard.c:490:SCardConnect() UnrefReader() count was: 3

_[36m00000180_[0m winscard_svc.c:451:ContextThread() CONNECT rv=0x0 for client 9

_[36m00008962_[0m _[34mhotplug_libudev.c:587:HPEstablishUSBNotifications() Device removed_[0m

_[36m00005891_[0m winscard_svc.c:317:ContextThread() Received command: TRANSMIT from client 9

_[36m00000314_[0m readerfactory.c:766:RFReaderInfoById() RefReader() count was: 2

_[36m00000164_[0m winscard.c:1581:SCardTransmit() Send Protocol: T=4

_[36m00000220_[0m _[34mAPDU: FF C2 00 00 07 80 03 01 00 00 81 00 00 _[0m

_[36m00000145_[0m _[34mifdhandler.c:1262:IFDHTransmitToICC() usb:1fc9/010b:libudev:0:/dev/bus/usb/002/003 (lun: 0)_[0m

_[36m00000375_[0m _[01;31mccid_usb.c:660:WriteUSB() write failed (2/3): -4 No such device_[0m

_[36m00000126_[0m _[34mSW: _[0m

_[36m00000141_[0m _[35mifdwrapper.c:527:IFDTransmit() Card not transacted: 617_[0m

_[36m00000310_[0m _[34mutils.c:68:SendHotplugSignal() Send hotplug signal to pcscd (pid=1288)_[0m

 

0 项奖励
回复

2,092 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please accept my apologies, but the implementation with emulated PICCs in mobile devices has not been tested and we cannot recreate the environment for this specific implementation.

Thank you for your comprehension.

BR,

Ivan.

0 项奖励
回复