PN7642 documentation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7642 documentation

Jump to solution
3,202 Views
ArtemPN
Contributor II

Hello! 

I`m using PN7642. I would like to read some documents containing IC`s peripheral detailed description and registers description. Also I would like to know if there are documents which describe bootloader communication protocol for FW programming via, for example, SPI interface. 

Can someone suggest where to look for such information? May be somewhere more related documents are available for PN7642? 

Thank you in advance!

Artem

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,171 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @ArtemPN

Hope you are doing well.

For more information about PN7642, you can consult the PN76 family instruction manual and UM11566 PN76 family NFC open controller user manual (since this document is under NDA, it is secured in Secure Files, and you will need to request access to it).

Regarding the firmware download, perhaps you may find useful the Secure Firmware Download example "DownloadLibEx1", which is available to demonstrate the secure firmware update by using LPC55 and MCUXpresso. You can find more information on this in PN76 family evaluation board quick start guide, Chapter 4 Software.

Regards,
Eduardo.

View solution in original post

0 Kudos
Reply
2 Replies
3,154 Views
ArtemPN
Contributor II

Thank you for reply. Now it is clear. I will try to sign NDA to be able to use this documentation.

 

0 Kudos
Reply
3,172 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @ArtemPN

Hope you are doing well.

For more information about PN7642, you can consult the PN76 family instruction manual and UM11566 PN76 family NFC open controller user manual (since this document is under NDA, it is secured in Secure Files, and you will need to request access to it).

Regarding the firmware download, perhaps you may find useful the Secure Firmware Download example "DownloadLibEx1", which is available to demonstrate the secure firmware update by using LPC55 and MCUXpresso. You can find more information on this in PN76 family evaluation board quick start guide, Chapter 4 Software.

Regards,
Eduardo.

0 Kudos
Reply