PN7462AU HSU UART – Is RTS/CTS Hardware Flow Control Enabled by Default

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462AU HSU UART – Is RTS/CTS Hardware Flow Control Enabled by Default

1,028 Views
uday_gowda
Contributor II

Hello Team,

I am working with PN7462AU, using HSU UART through HIF initialization. I would like to clarify whether RTS/CTS hardware flow control is enabled by default when using HSU UART on PN7462.

I am not explicitly enabling hardware flow control in firmware. However, I observed that UART transmission appears to depend on the CTS line state, and I would like to understand whether HSU/HIF internally enables or depends on RTS/CTS by default.

Questions:

  1. Is RTS/CTS hardware flow control enabled by default for HSU when phhalHif_Init() is called with E_HIF_HSU?

  2. Does phhalHif_Init() or HSU internally configure TX to wait for CTS?

  3. If flow control is enabled by default, how can it be disabled completely?

  4. Are there specific APIs or registers to disable RTS/CTS dependency?

My current HSU initialization is:

void Hif_UartInit(void)
{
    gHifConfig.eInterface = E_HIF_HSU;

    gHifConfig.sConfig.sHsuConfig.bIsHsuBoot  = 0;
    gHifConfig.sConfig.sHsuConfig.bBaudRate   = E_HSU_BAUDRATE_115_2K;
    gHifConfig.sConfig.sHsuConfig.bStopBits   = 1;
    gHifConfig.sConfig.sHsuConfig.bDummyBytes = 0;
    gHifConfig.sConfig.sHsuConfig.bEOF        = 32;

    gHifConfig.bTimeout       = 0;
    gHifConfig.eBufferType    = E_BUFFER_FORMAT_FREE;
    gHifConfig.bShortFrameLen = 0;
    gHifConfig.bStoreErrData  = 0;
    gHifConfig.bHeaderSize    = 0;

    phhalHif_Init(...);

    phhalHif_InitRxBuffer(...);
}

 

Any clarification would be helpful.

Thanks.

0 Kudos
Reply
3 Replies

1,009 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @uday_gowda

The host interface will sample the value of CTS before sending a byte; CTS must be in valid state for TX to proceed.

Perhaps you can try to "bypass" it by driving it to a fixed ready state. You could consider pulling CTS to the active state by using an external resistor.

Regards,
Eduardo.

0 Kudos
Reply

944 Views
uday_gowda
Contributor II

Hello @EduardoZamora 

Thank you for the clarification. Your explanation has given me a better understanding of how HSU communication depends on the CTS state before TX proceeds.

I understand the hardware workaround of pulling CTS to the active state externally. Could you please confirm if there is any register/API available to disable CTS dependency completely in software instead of using an external pull-down?

Thanks.

0 Kudos
Reply

837 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

My apologies, you would need to put CTS to active state by hardware.

Regards,
Eduardo.

0 Kudos
Reply