PN7462 Rf Callback

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462 Rf Callback

2,133件の閲覧回数
sachindia86
Contributor I

Hi NXP,

In PN7462 dev kit, DoorAccess Demo Example, we get a Rf Callback whenever a card is detected. Is it possible to get a callback whenever a card is removed from the reader?

Thanks

ラベル(2)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,085件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Once the card has been detected, there is not something like to check via RF. It is rather necessary to send some commands to verify if the Tag is still on the field. In the following thread there is the SW recommendation for this: https://community.nxp.com/message/1304209?commentID=1304209#comment-1304209 

Hope it helps!

BR,

Ivan.

0 件の賞賛
返信

2,085件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Once the card has been detected, there is not something like to check via RF. It is rather necessary to send some commands to verify if the Tag is still on the field. In the following thread there is the SW recommendation for this: https://community.nxp.com/message/1304209?commentID=1304209#comment-1304209 

Hope it helps!

BR,

Ivan.

0 件の賞賛
返信