PN7462: Register for current DPC Gear

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462: Register for current DPC Gear

1,711件の閲覧回数
johannesdev
Contributor III

Hi,

were are currently developing an application using the PN7462 with 4 DPC gears. Is it possible to read the current gear from a register (when the field is active of course)?

The NFC cockpit has the desired function implemented, but I don't have any clue how to read it within the C application based on the Reader-Lib.

johannesdev_0-1634726570415.png

Thanks and best regards,
Johannes

 

0 件の賞賛
返信
1 返信

1,690件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @johannesdev ,

 

You may have the current AGC value from the following register.

Kan_Li_0-1635326371946.png

but have to calculate the current gear number with help of high/low AGC threshold for each gear, as well as the gear size, gear step size and start gear number. Please kindly refer to https://www.nxp.com/docs/en/application-note/AN11742.pdf for more details.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 件の賞賛
返信