Hi Everybody,
for a NFC Access System we need some USB-Desfire Readers. So we choose the PN7362. It works fine with the Software Example phEXNFCCid from the latest SW368334 Package. But to improve the performance we want to disable the LEDs and improve the Polling Frequency. But i dont know where it could be changed.
Thanks for you Help and best Regards
flesky
@EduardoZamora Hi Thank you Eduardo, that helps a lot
could you help me to configure a faster polling loop? for our application it would be better to access the desfirecards as soon as possible. Thank you very much
flesky
Hi,
Could you please provide more details? Are you looking for a way to reduce the time between each polling?
Any additional information is really appreciated.
Regards,
Eduardo.
Hi @EduardoZamora ,
thanks, yes we are searching for a way to polling duration . So we need to improve the polling rate. ATM it seems to be every 500ms. It it possible to set it to 100 to improve the tag detection?
thanks for you help and best regards
flesky
Hi,
As mentioned in PN7462AU PC CCID Reader User Manual, Section 1.3 "phExNFCCcid" example, this application has the following modules:
CL Task can be found in phExNFCCcid.c file; static void phExNFCCcid_ClifTask(void *pvParams) configures discovery loop parameters and should also configure poll timer.
Regards,
Eduardo.
thanks for you help. I think the wWakeUpTimerVal is the way to imporove the Reading time. So i changed the Register in the eeprom. from 300 to 100 on adress 0x201300 so i think this is right?
Best regards
Hi,
We may not have any demo that meets your requirements; however, if your application focuses only on specific card technologies, I recommend removing the cases/conditionals/portions of code related to the technologies that are not relevant for your project from the discovery loop.
Please notice that PN7362 does have a listen mode in the application and, in case you are not using it, you may also remove it.
Unfortunately, we do not have any guides for implementing this, and I will strongly recommend testing different scenarios since your application requirements involve not only NFC, but also USB.
Regards,
Eduardo.
Hi,
thank you very much. I am not good at programming, do you know where i can disable the listen mode part? is there a easy way to disable it? For our application we need only PCSCD > Contactless cards. No Contacted Interface, no special Mifare code, no listen/p2p.
Thank you very much
best regards
Flexy
Hi Eduardo, do you know where i disable the polling of Felica, P2P and other techniques on the Program? We need only the detecting and use of Type A Cards.
if i remove remove it from the APP_NxpBuild.h there comes many compile errors. So this is not the right way. Could you help me in this case?
Big Thank you
Best regards
Hi,
I truly apologize for the late response; we are under a great load of work.
My apologies, we may not have any demo or specific guide about what you are trying to achieve. I would recommend taking a look at the MIFARE Classic example from the NFC Reader Library and compare the structure and the application flow against the phExNFCCcid example.
As mentioned before, you can find some hints in the PN7462AU PC CCID Reader User Manual. The application consists of the following modules:
You can find some helpful information about the Reader Library API and devices specific API inside NfcRdLib folder > docs.
Please, try making some changes as required by your project in the relevant modules and previously mentioned tasks/functions. After performing your tests, please let me know your findings.
Please, allow me to apologize again for the delay and the inconvenience this might cause you.
Regards,
Eduardo.