PN7221 adaptation for Android 16

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7221 adaptation for Android 16

897 Views
zhangkai
Contributor II

Could you please advise whether "AN14880 PN7160/PN7220 - Android 16 porting guide" is applicable to the PN7221 chip?

If not applicable, please provide the documentation for porting PN7221 to Android 16.

Tags (1)
0 Kudos
Reply
2 Replies

524 Views
zhangkai
Contributor II

@KaiLi 

The chip type read by the HAL layer is PN7220, as shown in the following logs:
 
07-01 02:08:17.400 518 5053 D NxpHal : processChipType Setting Default ChiptType pn7220
 
07-01 02:08:17.400 518 5053 D NxpHal : processChipType Product : pn7220
 
07-01 02:08:17.400 518 5053 D NxpHal : phNxpNciHal_configFeatureList ()chipType = 4
 
07-01 02:08:17.400 518 5053 D NxpTml : phTmlNfc_e_setFragmentSize 0x22A
 
 
However, the actual silkscreen marking on the chip is PN7221.
zhangkai_0-1782900299716.jpeg

 

Could you advise whether NXP_NFC_HW in device-nfc.mk should be configured as pn7220_i2cs or pn7221_i2cs?
0 Kudos
Reply

881 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @zhangkai 

The "AN14880 PN7160/PN7220 - Android 16 Porting Guide" applies to both PN7220 and PN7221.

0 Kudos
Reply