PN5xx I2C kernel mode driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5xx I2C kernel mode driver

3,110 Views
sivasu4098
Contributor III

hi all,

For PN7150 is supportable with PN5xx i2c kernel driver. I want to know that PN544 is compatible with PN7150. Orelse any supporting drivers for PN7150. Please specify it.

Thanks and Regards,

Sivasubramaniyan P

0 Kudos
Reply
2 Replies

2,101 Views
sivasu4098
Contributor III

Hi,

I am trying to port PN7150 to Android Nougat, So with PN5XX kernel driver will create the device node  /dev/pn544 and then using this /dev/pn544 it is possible to read and write the NFC Tags.

Thanks and Regards,

Siva

0 Kudos
Reply

2,101 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

    PN544 is designed for mobile phone, we have special team(mobile team) to support it. PN7150 & PN544 uses the same driver, which doesn't mean they are fully compatible to each other.

  

Have a nice day!

BR,

Weidong

0 Kudos
Reply