PN532 InDataExchange analog in PN7150

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN532 InDataExchange analog in PN7150

3,597 Views
superoriginalma
Contributor I

I am porting in-house library for reading desfire tags from old reader (PN532) to newer one(PN7150). This library works over InDataExchange command of PN532. I am not sure if I understood what is corresponding command for PN5170. As I understood this IC should be configured to use protocol ISO DEP and Interface ISO DEP with RF_DISCOVER_MAP_CMD, and then it should be put into discovery mode with RF_DISCOVER_CMD. After that I can send data packets, and those commands that was previously handled by InDataExchange command should be put into payload. Did I got it right? Are there any libraries that demonstrate how to properly use ISO DEP protocol? I am still not sure whether I should use ISO DEP , NFC DEP or RF Frame protocols.

Labels (1)
Tags (3)
0 Kudos
Reply
3 Replies

3,322 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

According to Table 4 of PN7150's User Manual, PN7150-NCI supports ISO-DEP (Reader/Writer): 

https://www.nxp.com/docs/en/user-guide/UM10936.pdf

It would be helpful to refer to NCI pdf file available under registration in NFC Forum, which describes better the RF Communication Configuration.

Regards,

Ivan.

0 Kudos
Reply

3,322 Views
superoriginalma
Contributor I

Thanks for update. Could you please provide the link to the document you mentioned?

0 Kudos
Reply

3,322 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

First register in NFC Forum and then make a search for the NCI document.

NFC Forum:

https://nfc-forum.org/ 

Regards,

Ivan.

0 Kudos
Reply