PN532-Desfire NFC Card error response

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN532-Desfire NFC Card error response

2,103 Views
adityajain
Contributor I

Hello,

I am trying to authenticate a Desfire Card using PN532 NFC reader, I am using HSU mode. 

Here are the commands and there response from the card

(Initialization Command)

Command 1: 55 55 00 00 00 00 FF 02 FE D4 02 2A 00 

Response : 00 00 FF 06 FA D5 03 32 01 06 07 E8 00  

(SAM Config) 

Command 2:  55 55 00 00 00 00 FF 05 FB D4 14 01 14 01 02 00

Response : 00 00 FF 02 FE D5 15 16 00

(Read Card ID)

Command 3:  00 00 FF 04 FC D4 4A 01 00 E1 00

Response : 00 00 FF 15 EB D5 4B 01 01 03........... (card ID)

(Authentication Command 1)

Command 4: 00 00 FF 0C F4 D4 40 01 90 5A 00 00 03 00 00 00 00 FE 00

Response : 00 00 FF 03 FD D5 41 01 E9 00 (i.e error)

Is there some problem with my code of with the PN532.

Tags (3)
0 Kudos
Reply
0 Replies