PN5180 into 14443B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5180 into 14443B

1,788 Views
liyanping
Contributor I

hello ,nxp teams.I  want to configure pn5180 into 14443B without Reader-Library. What is the logical flow.

I reference the document(AN12650pdf--Using the PN5180 without library) and I write my code flow, but it no success. please tell me how to do.

0 Kudos
Reply
4 Replies

1,181 Views
Nadernader
Contributor I

My question is the same.
Does anyone know the answer to this question?

@fangfang 
@liyanping 

 

0 Kudos
Reply

1,778 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Did your PN5180 can communicate with Host via SPI? Would you please double check it?

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

Tags (1)
0 Kudos
Reply

1,762 Views
liyanping
Contributor I

do you have any solution?

0 Kudos
Reply

1,772 Views
liyanping
Contributor I

yes,host MCU is stm32,stm32 communicate with pn5180 via SPI, my host can read pn5180  eeprom data, i  am sure that . And I configure pn5180 into 14443A , it can read A Card message. But I don't know how to configure into 14443B.

Tags (1)
0 Kudos
Reply