PN5180 ISO15693 ICODE SLIX read NDEF sections ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5180 ISO15693 ICODE SLIX read NDEF sections ?

2,515 Views
Alansbor77
Contributor I

Hi All !

Can you please tell me how to read using PN5180 ISO15693 ICODE SLIX - NDEF sections?

The guys used to answer me about reading a lot of labels without collisions, they gave the SPI pseudo code, maybe there is such a thing here?

Please tell me where can I read, see, try?

Alex.

 

 

Tags (1)
0 Kudos
Reply
2 Replies

2,504 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello @Alansbor77 .

Please kindly refer to 

NFC Reader Library: Software Support for NFC Frontend Solutions 

for the detail code example.

Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply

2,500 Views
Alansbor77
Contributor I

Hello fangfang
Thanks a lot for the link, I went to study.

Alex

 

0 Kudos
Reply