PN5180 IRQ PIN In Library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN5180 IRQ PIN In Library

2,221件の閲覧回数
smiwa
Contributor III

Hi,

I have a question about IRQ pin setting for PN5180. Its datasheet says IRQ pin can be configured by the register IRQ_PIN_CONFIG (01Ah).

I am using Library (NFCReaderLibraryForPNEV5180B-04.030.00.011627) bun I cannot find that which polarity, active low or active high, IRQ pin configuration is set in that library. 

Could you please let me know where and when it is configured in the library software?

Thank you for your help!

Best regards,

   S. Miwa

0 件の賞賛
返信
2 返答(返信)

1,845件の閲覧回数
smiwa
Contributor III

Hi Isaac san,

Sure. Thank you very much!

Best regards,

   S. Miwa

0 件の賞賛
返信

1,846件の閲覧回数
isaacavila
NXP Employee
NXP Employee

Hello,

You may refer to this thread: https://community.nxp.com/thread/437631 

Regards,

Isaac

0 件の賞賛
返信