PN5180 IRQ PIN In Library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5180 IRQ PIN In Library

2,226 Views
smiwa
Contributor III

Hi,

I have a question about IRQ pin setting for PN5180. Its datasheet says IRQ pin can be configured by the register IRQ_PIN_CONFIG (01Ah).

I am using Library (NFCReaderLibraryForPNEV5180B-04.030.00.011627) bun I cannot find that which polarity, active low or active high, IRQ pin configuration is set in that library. 

Could you please let me know where and when it is configured in the library software?

Thank you for your help!

Best regards,

   S. Miwa

0 Kudos
Reply
2 Replies

1,850 Views
smiwa
Contributor III

Hi Isaac san,

Sure. Thank you very much!

Best regards,

   S. Miwa

0 Kudos
Reply

1,851 Views
isaacavila
NXP Employee
NXP Employee

Hello,

You may refer to this thread: https://community.nxp.com/thread/437631 

Regards,

Isaac

0 Kudos
Reply