Hello,
I bought a PN5180 Evaluation board, and from the quick start guide I am trying to setup the board.
In the directions in section 3.2.3 (option 2) it says replace the file on the board with an updated bin file. I managed to do that and the device restarts, but afterwards I still cannot connect to NFC Cockpit.
I have installed the drivers that came in the VCOM folder. But when I check device manager it is still saying it is a USB Serial device (in fact its saying it is 2 devices for some reason).
Is there an additional driver I am missing? I also tried to connect to MCUXpresso but I couldn't connect to that either.
Thank you for any assistance that can be provided