PN5180 Card emulation function question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5180 Card emulation function question

2,338 Views
chlee2
Contributor I

Hi.

The card emulation function of PN5180 is review.

Regarding the iPhone and card emulation function,

The iPhone is a card reader, and the application with PN5180 can communicate with the iPhone through Felica type, and I would like to ask if it is possible to process it in F/W with a specific data value.

0 Kudos
Reply
1 Reply

2,245 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

The PN5180 frontend IC supports the following RF operating modes:


• Reader/Writer mode supporting ISO/IEC 14443 type A up to 848 kBit/s
• Reader/Writer communication mode for MIFARE Classic contactless IC
• Reader/Writer mode supporting ISO/IEC 14443 type B up to 848 kBit/s
• Reader/Writer mode supporting JIS X 6319-4 (comparable with FeliCa scheme)
• Supports reading of all NFC tag types (type 1, type 2, type 3, type 4A and type 4B)
• Reader/Writer mode supporting ISO/IEC 15693
• Reader/Writer mode supporting ISO/IEC 18000-3 Mode 3
• ISO/IEC 18092 (NFC-IP1)
• ISO/IEC 21481 (NFC-IP-2)
• ISO/IEC 14443 type A Card emulation up to 848 kBit/s

You can check more details about this in the Datasheet of the device. The device does not list the Felica Type in the card emulation mode.

You can emulate a type A card and read it with the phone.

Hope that helps.

Regards,

Estephania

0 Kudos
Reply