NxpRdLib or NxpRdLibNet PCSC Example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NxpRdLib or NxpRdLibNet PCSC Example

2,577件の閲覧回数
moh_m
Contributor I

is there a complete example for using NxpRdLib/NxpRdLibNet with desfire EV1/EV2 Cards with/without SAM using a PCSC reader, the example should have creating Applications and Files and read/write them.

0 件の賞賛
返信
1 返信

2,444件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hope you are doing great, 

for PC/SC readers you can check the export controlled library and use it as reference since it is intended to work with our PEGODA reader, but this ( export controlled, SAM and DESFire)  is secured under NDA ( Non Disclosure Agreement) which means that all the information, tools and support should be delivered using secured communication channels and only to customers with active NDA.

 this is a public forum where we should not discuss  this type of topics. please contact your Distributos or NXP contact in order to get an NDA or the SW available in docsotre.

Have a great day!

BR

Jonathan

0 件の賞賛
返信