Nt3h2111 Sample Code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Nt3h2111 Sample Code

7,108 Views
robertosocorreg
Contributor I

Hi, 

Does anybody have any sample code for the Nt3h2111? I'm interested in the pass-through mode of the Nt3h2111. Any suggestions are greatly appreciated. A sample code to setup the tag by I2C will make my life easier with a project that I'm working on.

Thank you, 

Robert

0 Kudos
Reply
3 Replies

5,460 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Roberto Socorregut,

You can refer to the example code for OM5569-NT322E evaluation kit. Please find it in the "Downloads" tab in the next link:

OM5569-NT322E | NTAG I2C plus Explorer Kit | NFC|NXP 

For prototyping or evaluation I would recommend you to get the kit. The NTAG I2C Plus driver code is for LPC MCUs, but it can be easily ported to any MCU since it consists of simple I2C commands.

In case of any doubts do not hesitate to ask in this community.


Best Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,460 Views
sha_lu
Contributor I

Hi Jorge_Gonzalez,

I looked at sample code of NFC I2C Plus,  it likes only work for NXP MCUs,  Does nxp provide any sample code for linux or freeRTOS MCU platforms?  Thanks

BR

Scott

0 Kudos
Reply

5,460 Views
salihtopal
Contributor I

Hi Jorge,

I have a new project and i use NT3H2111.

Is device address 0x55? 

I'm not sure device address. My address is incorrect or my i2c configuration is wrong. I send only slave address and then one byte. 

0 Kudos
Reply