NfcrdlibEx8_HCE_T4T example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NfcrdlibEx8_HCE_T4T example

1,455 Views
nddona
Contributor I

We have a custom Linux platform where we have successfully made the PN5190 to work as a card reader for years.

Now we want to try out to make it work as a type 4A tag as in example "NfcrdlibEx8_HCE_T4T". We have tried to use the example with the reader library version 7.14.00 but we're getting the same results as reported in the thread: https://community.nxp.com/t5/NFC/HCE-T4T-Example-not-working-with-NXP-NFC-Library-v07-08-00-in/td-p/...

When Android (Samsung S23 ultra) is tapped with NXP "TagInfo" App, it's getting an invalid RATS. Rx buffer receives data starting with 0x11 0xD4 ... etc.

[phacDiscLoop_Sw_Run] Starting Listen Mode
[T4TCardEmulation] Card Activated in Listen mode...
[phpalI14443p4mC_Sw_Activate] RATS: 11 D4 00 8C 26 82 9B FA 12 01 DF 84 5B 00 00 00 30
[phpalI14443p4mC_Sw_Activate] Invalid RATS received...

 

Is it because the phone is trying to talk in NFC-DEP (P2P Mode / SNEP)? 

Appreciate any help to resolve this issue.

Thanks!

0 Kudos
Reply
4 Replies

1,147 Views
nddona
Contributor I

Hi,

I have further question related to this topic.

Even though I got our device to work as a type 4 card emulator with "NfcrdlibEx8_HCE_T4T" example, it seems very slow. The application steps are as below.

1. Device runs in the reader (polling) mode

2. A phone is tapped and it reads a card in mobile wallet

3. Immediately turns off RF after reading finishes

4. Re-initialize the RF chip in HCE type 4 card emulator mode (passive listener mode)

5. Sends a URL (NDEF) to the smart phone

The issue is it takes about 1500ms to re-init the RF chip in card emulator mode and send the URL to smartphone.

Is there a faster way to do this, so that user doesn't have to keep the phone holding/tapping ?

When I searched on Google it says that it can be done via type 2 tag as below. But it didn't work. Nothing was received by the phone.

│
▼
Step 1: Terminate Field 
│ (~1ms)
▼
Step 2: Load NDEF Data 
│ (~3ms)
▼

Step 3: Go Autocoll 

Appreciate if you can guide me on how exactly I can achieve this fast mode switching and a URL is sent to a phone within 500ms.

Thanks!

0 Kudos
Reply

1,134 Views
nddona
Contributor I

In related to my question above, the code I tried to implement after terminating the field as given below. I can get phhalHw_Autocoll() to return success but I get 0x020A for phhalHw_Pn5190_Instr_ExchangeRFData(). 

phhalHw_Pn5190_Autocoll() is also updated with the below.

phhalHw_Pn5190_Instr_SwitchModeAutocoll(pDataParams,bRfTechnology,PHHAL_HW_PN5190_AUTOCOLL_MODE_AUTONOMOUS_WITH_STANDBY))

 

int card_emulator_main_cutdown(void)

{

    do

    {

        int               ret;

        phStatus_t        status;

        pHal_Hce = phNfcLib_GetDataParams(PH_COMP_HAL);

        TRACE0("NfcLib data params pointers set successfully");

 

        /* ================================================================= */

        /*   STEP 3: STAGE EMULATION PROFILE AND LOAD URL PAYLOAD        */

        /* ================================================================= */

        TRACE0("Configuring hardware target layers and loading URL buffer...");

       

        /* Configure target mode HAL parameters */

        status = phAppHce_HALConfigAutoColl();

        CHECK_STATUS(status);

        if (status != PH_ERR_SUCCESS) {

            TRACE1("phhalHw_TargetInit failed: 0x%04X", status);

            return status;

        }

        /* ================================================================= */

        /*   STEP 4: ENGAGE AUTOCOLL (Autonomous Listening State)         */

        /* ================================================================= */

        TRACE0("Entering sub-100ms Autonomous Listen mode...");

       

        // CRITICAL FIX: Allocate valid storage memory to prevent PH_ASSERT_NULL crashes

        uint8_t * pRxBufferPtr = NULL;

        uint16_t  wRxLengthData = 0;

        uint16_t  wProtocolParams = 0;

        // Execute the function mapping strictly to your HAL's parameter footprint.

        // We pass 'A_MODE' to tell the switch code to select Passive NFC-A Technology.

        status = phhalHw_Autocoll(

            pHal_Hce,

            A_MODE,             // Bitmask flag forcing NFC-A technology profiling

            &pRxBufferPtr,      // Passed as a valid pointer reference to a pointer

            &wRxLengthData,     // Passed as a valid pointer reference to length

            &wProtocolParams    // Passed as a valid pointer reference to parameters

        );

        if ((status & PH_ERR_MASK) == PH_ERR_SUCCESS) {

            TRACE0(" Tap-to-URL switch executed perfectly! Phone hit the antenna field.");

            TRACE1("De-wrapped Activation Protocol Parameters: 0x%04X", wProtocolParams);

            /* ================================================================= */

            /*   STEP 5: PROCESS INCOMING APDU COMMANDS FROM THE PHONE         */

            /* ================================================================= */

            TRACE0("Listening for phone file system read commands...");

           

            // Allocate data exchange buffers

            uint8_t * pDataIn = NULL;

            uint16_t  wDataInLen = 0;

            // Retrieve the initial data packet the phone transmitted right upon activation

            // Your Autocoll snippet already stores the address in pRxBufferPtr / wRxLengthData

            pDataIn = pRxBufferPtr;

            wDataInLen = wRxLengthData;

            // Enter a rapid loop to process the phone's Read commands

            // The phone will send "Select NDEF Application" -> "Select NDEF File" -> "Read Binary"

            //while (1)

            {

                //Use the correct Target Emulation transmit function to bypass the 0x0225 check

                //PH_RECEIVE_RF_ENABLE_EVT_STATUS enables event tracking for the transfer

                status = phhalHw_Pn5190_Instr_ExchangeRFData(

                    pHal_Hce,

                    PH_EXCHANGE_DEFAULT,                  // wOption

                    0,                                    // bTxLastBits (0 indicates complete 8-bit byte layout)

                    0x05,                                 // bRespControl: Bitmask 0x04 (Event Status) | 0x01 (Rx Status)

                    aNdefFile,                            // Your URL array structure

                    23,                                   // Size of your URL data payload

                    &pRxBufferPtr,                          // Address of your response data pointer

                    &wRxLengthData                        // Address of your incoming length tracker

                );

           

                if (status == PH_ERR_SUCCESS) {

                    TRACE0(" Single-shot URL packet injected successfully. Task complete!");

                } else {

                    TRACE1("Injection status / timeout: 0x%04X (Phone likely disconnected cleanly)", status);

                }

            }

        } else {

            TRACE1("Autocoll exited, timed out, or dropped with status: 0x%04X", status);

        }

    } while(0);

    return 0;

}

 

// /* Mandatory NDEF file. It's set using phceT4T_SetElementaryFile. */

uint8_t aNdefFile[] = {

    /* --- MANDATORY CONTACTLESS TRANSPORT HEADER --- */

    //0x02,       // 1. PCB Byte: Configures this frame as a Part 4 I-Block (Block Number 0)

    0x00, 0x13, // 1. T4T Container Length Indicator (19 bytes total payload)

    0xD1,       // 2. NDEF Record Header (MB=1, ME=1, SR=1, TNF=0x01 Well-Known Type)

    0x01,       // 3. Type Length (1 byte long name)

    0x0F,       // 4. Payload Length (15 bytes for prefix + string)

    0x55,       // 5. Record Type: 'U' (0x55 for URI record)

    0x02,       // 6. URI Identifier Prefix: Code 0x02 maps to "https://www."

   

    // 7. URI Payload String of 14bytes

    0xww, 0xww, 0xww, 0xww, 0xww, 0xww, 0xww, 0xww, 0xww, 0xww, 0xww, 0xww, 0xww, 0xww,

     /* --- MANDATORY SMART CARD STATUS TRAILER --- */

    0x90, 0x00  // 21-22. APDU Success Status (tells Android the data read is complete)

};

Log output:

06-16 17:34:31.600 26047 27687 E nfc : [card_emulator_main_cutdown] NfcLib data params pointers set successfully

06-16 17:34:31.600 26047 27687 E nfc : [card_emulator_main_cutdown] Configuring hardware target layers and loading URL buffer...

06-16 17:34:31.605 26047 27687 E nfc : [card_emulator_main_cutdown] Entering sub-100ms Autonomous Listen mode...

06-16 17:34:31.607 26047 27999 V nfc : [socket_send_thread] Entered socketSend

06-16 17:34:31.607 26047 27999 V nfc :

06-16 17:34:32.456 26047 27687 E nfc : [card_emulator_main_cutdown] Tap-to-URL switch executed perfectly! Phone hit the antenna field.

06-16 17:34:32.456 26047 27687 W nfc : [card_emulator_main_cutdown] De-wrapped Activation Protocol Parameters: 0x0100

06-16 17:34:32.456 26047 27687 E nfc : [card_emulator_main_cutdown] Listening for phone file system read commands...

06-16 17:34:32.456 26047 27687 W nfc : [card_emulator_main_cutdown] Injection status / timeout: 0x020A (Phone likely disconnected cleanly)

 

 

0 Kudos
Reply

1,401 Views
nddona
Contributor I
This issue is solved by disabling some macros and updating the SAK to correct value 0x20.
0 Kudos
Reply

1,350 Views
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir,

Thank you for letting me know. I will address this for the respective clarifications and updates.

Have a great day!

Best Regards,
Fabian
0 Kudos
Reply