NXP PN5180 NFC support on Android Oreo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP PN5180 NFC support on Android Oreo

3,941 Views
dhrumildoshi
Contributor III

Hello All,

I am working  on a Point of Sale terminal system. It has Android Oreo 8.0 OS installed on a custom board. 

We have put NXP's PN5180 NFC chip in hardware design for the payment purpose. 

I need to add kernel drivers and NFC library in the software for the chip to access it from the Android's APK level.

So, I need full step by step documentation for the same and also required software drivers and libraries download links.

Please let me know if it is possible to add support for PN5180 NFC chip in Android Oreo OS. If so, please provide required/requested details.

Thanks & Best Regards,

Dhrumil

Labels (1)
0 Kudos
Reply
4 Replies

3,374 Views
jimmychan
NXP TechSupport
NXP TechSupport

We don’t have android support for PN5180 however the NxpReaderLibrary available on Linux can be easily ported to Android environment (just requires makefiles adaptation). It won’t rely on Android AOSP NFC service but a native application can be created based on the NxpReaderLibrary.

You can find the App. Notes from here:

PN5180 | NFC Frontend IC for POS terminals|NXP 

0 Kudos
Reply

3,374 Views
dhrumildoshi
Contributor III

Hi Jimmychan,

Thanks for your response.

We need a solution which is compatible with Android AOSP NFC service on Android Oreo. In last week, I came across NXP PN7150 NFC chip and it seems that the drivers for chips can be easily ported on Android Oreo. Please confirm if it can be ported on Android Oreo. If so, Please provide development guide for porting drivers for PN7150 in Android Oreo AOSP.

Please let me know if you have suggestion for any other chip from NXP which has support for Android Oreo.

I would appreciate a quick response.

Thanks again,

Dhrumil

0 Kudos
Reply

3,374 Views
jimmychan
NXP TechSupport
NXP TechSupport

Yes, PN7150 support Android Oreo.

You can get the patch from here:

GitHub - NXPNFCLinux/nxpnfc_android_oreo: Android patches for support of PN7150 NCI based NXP NFC Co... 

You can download the App. Notes from here:

PN7150|High performance NFC controller for home automation|NXP 

0 Kudos
Reply

3,374 Views
dhrumildoshi
Contributor III

Hello All,

I would appreciate a response on the above query.

Thanks,

Dhrumil

0 Kudos
Reply