NTP5332 Event Detection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NTP5332 Event Detection

2,347件の閲覧回数
jtem1976
Contributor I

I am having difficulty setting my NTP5332 to send signals that events have been detected. I have tried the following in Android but can't seem to get the card to respond.  I get an error code of 0x01 

Does anyone have the right sequence of bytes to send?

 

public static final byte[] cmd_activateEDPinAl = new byte[]{
(byte) 0x12,
(byte) 0xC1,
(byte) 0x04,
(byte) 0x3D, //Config Memory for ED/EH Pin
(byte) 0x01, // EH_CONFIG
(byte) 0x00, // RFU
(byte) 0x01, // ED_CONFIG - Start Any command 00001010
(byte) 0x00

};

public static final byte[] cmd_activateEDPin = new byte[]{
(byte) 0x12,
(byte) 0xC1,
(byte) 0x04,
(byte) 0xA8, //Config Memory for ED/EH Pin
(byte) 0x01, // ED_CONFIG - Start Any command 00001010
(byte) 0x00, // RFU
(byte) 0x00,
(byte) 0x00

};


public static final byte[] cmd_clearEDPin = new byte[]{
(byte) 0x12,
(byte) 0xC1,
(byte) 0x04,
(byte) 0xAB, //Config Memory for ED/EH Pin
(byte) 0x01, // Clear 00000001 -> 0x01
(byte) 0x00, // RFU
(byte) 0x00, // RFU
(byte) 0x00 // RFU
};
0 件の賞賛
返信
3 返答(返信)

2,140件の閲覧回数
trueBlue20022
Contributor I

Hi. fangfang,

 

I am unable to find the above reference manual RM00221.pdf by following the link

 

Thanks

 

 

0 件の賞賛
返信

2,141件の閲覧回数
trueBlue20022
Contributor I

Hey fangfang, I am not able to find the above link RM00221.pdf file. Can you please report?

0 件の賞賛
返信

2,334件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

You may refer to  the reference manual as the link for the more information.

URL:https://www.nxp.com.cn/docs/en/reference-manual/RM00221.pdf.

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信