NTAG based Systems - Regulatory Testing Requirements - FCC / CE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NTAG based Systems - Regulatory Testing Requirements - FCC / CE

2,040件の閲覧回数
davidsherrets
Contributor I

Normally an RFID / NFC tag is a considered a passive device and FCC testing is not required.  

 

However,

When you add a microcontroller and other peripherals that start clocking at different frequencies than the 13.56 carrier frequency, experience says that you get an unintentional radiator.    

1. So the question is do systems as described above require FCC and/or CE Testing?

2. If not, please explain why these are not considered unintentional radiators? 

 

3. Also - why does the the NTAG Demo board contain an FCC-ID: OWROM5569-NT322E. 

Thanks for your help.

0 件の賞賛
返信
1 返信

1,874件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi David,

If a system involved MCU and oscillation circuit then FCC is required.
For our OM5569 demo set, it included two part, one is NTAG I2C plus board, and the other is LCD displayer which embedded with LCD display, MCU and sensor that required FCC certification.


Hope that makes sense,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信