NTAG 424 encrypted file data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NTAG 424 encrypted file data

ソリューションへジャンプ
3,739件の閲覧回数
MPucci
Contributor III

Hello community,

talking about NTAG424 and SDMENCFileData: is it possible to add to static file data a random padding? The goal is to have at any NDEF reading a different value, because even if the mirror is crypted, is always the same.

Thanks

Mario

0 件の賞賛
返信
1 解決策
3,685件の閲覧回数
MPucci
Contributor III

Hi Fabian,

my fault. I discovered that my enc data was just an encryption of static file without the algorithm inside ntag. Maybe i messed up the offsets that prevents the algorithm to work properly.

Thanks

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,686件の閲覧回数
MPucci
Contributor III

Hi Fabian,

my fault. I discovered that my enc data was just an encryption of static file without the algorithm inside ntag. Maybe i messed up the offsets that prevents the algorithm to work properly.

Thanks

0 件の賞賛
返信
3,671件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

No problem. I'm glad you were able to identify the root cause.

Best Regards,
Fabian
0 件の賞賛
返信
3,713件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello, my name is Fabian, I've been assigned to support your case.
Thank you for your interest in our products.
SDMENCFileData is already an encrypted file, its structure and format are defined by some proprietary security mechanisms. For this reason, the encryption protocol used typically includes padding schemes, these are implemented in order to meet specific block sizes.
Unfortunately, since there are some proprietary implementations, we cannot share any specifics regarding this procedure.

Best Regards,
Fabian
0 件の賞賛
返信
3,701件の閲覧回数
MPucci
Contributor III

Thanks Fabian,

i've all the info necessary to decrypt it from the NDEF message. My problem is different if i understood correctly the documentation: take for example page 13 of AN12196. The StaticFileData is 7878787878787878778.... and the corresponding SDMENCFileData is 94592FDE69FA06E8E3B6CA686A22842B. This value of SDMENCFile data is fixed, i mean is always the same at every read of NDEF. This can lead a malicoius to think that in this position there is a static data, even if encrypted. I'd like to change the SDMENCFiledata at every read with "Static data + random data". From my algorithm, once decripted i know where is the static and where is the random.

0 件の賞賛
返信