NTAG 210µ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTAG 210µ

1,768 Views
raymondh
Contributor I

I understand that NTAG 210µ on the Internet, want to know which of the 210µ refers to NFC chip thickness? Or what? If the information is embedded, what formats and devices are read by the chip?

Tags (2)
0 Kudos
Reply
1 Reply

1,666 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Huang,

      You can get all information of NTAG 210u from the link:

NT2L1001_NT2H1001|NXP 

      NTAG 210μ is designed to comply fully with NFC Forum Type 2 Tag and ISO/IEC14443 Type A specifications, so all NFC readers that support ISO/IEC14443 Type A can be reader for the Tag.

      Materials for NFC reader are here:

NFC Reader ICs|NXP 

      you can select one of them, such as MFRC 630, CLRC663 etc.

Have a nice day!

Best Regards,

TIC Weidong

0 Kudos
Reply