NTA5332 How To Restore

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTA5332 How To Restore

1,490 Views
fei6688
Contributor I

When using the NTA5332 for development, the NFC read/write configuration file has been set to disable via nfc. After that, an I2C abnormality caused communication failure with I2C. After recovery, communication with the NTA5332 via I2C is not possible, and NFC can no longer be configured. Is there any way to restore it to factory settings? It is suspected that the I2C abnormality caused an issue in the configuration, and I2C communication remains unavailable.

0 Kudos
Reply
2 Replies

1,419 Views
jimmychan
NXP TechSupport
NXP TechSupport

Do you mean the I2C bus stuck?  Have you try the I²C bus recovery (9 SCL pulses)? 

0 Kudos
Reply

1,402 Views
fei6688
Contributor I

No,If neither the I2C nor the NFC interface of the NTA5332 chip can communicate, it may be due to incorrect configuration of the chip. Are there any methods to restore it to factory settings?

0 Kudos
Reply