NT3H2111 Is there difference in readrange powered from RF-field or host

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NT3H2111 Is there difference in readrange powered from RF-field or host

1,467 Views
arnodegroot
Contributor I

We use the NT3H2111 without energy harvesting, so nothing is connected to the Vout pin.

Is there any difference in readrange when the chip is: powered from RF-field first (without applying external power from the host), or when the chip is powered from the host first and then brought into the RF-field?

11 Communication and arbitration between NFC and I2C interface

"If both interfaces are powered by their corresponding source, only one interface shall

have access to the memory according to the "first-come, first-serve" principle."

0 Kudos
Reply
1 Reply

1,389 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear Arno de Groot,

There should not be any difference in the read range, this device is still a passive element, so the read range  is the same for both cases, the section you refer here  talks about the arbitration of the EEPROM  in case that the RF interface try to  write or read from the EEPROM at the same time as the I2C interface. there is an arbitration to avoid this kind of collision.

BR

Jonathan

0 Kudos
Reply