NHS 3152 current reading

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NHS 3152 current reading

2,630 次查看
joohee710610
Contributor I

Hello, everyone.

I want to read the current of a sensor using the NHS 3152.

I already had a NHS 3152 starter kit. 

However, I don't understand the datasheet because my major is in materials science.

Therefore, I have many wondering. 

First, I think that the sensor needs to connect to the pin to read current. What number of the pin is connected to the sensor? 

Second, I need to code the chip to read current. Are any open sources to read current of the sensor? 

0 项奖励
回复
3 回复数

1,541 次查看
HafizUsman
Contributor I

Hi Joohee,

I am working on the same type of academic assignment these days. I have NHS3152 board and I want a chip code for current measurements. Please guide me if you completed your activity.

Thank you

0 项奖励
回复

2,522 次查看
driesmoors
NXP Employee
NXP Employee

Hi,

The NHS3152 contains 6 analog lines that can be connected to the I2D (current-to-digital) HW block. You will need to write a C code that runs on the ARM processor in the NHS3152 IC to connect the lines internally to the I2D HW block, to power and clock the I2D block, to configure it and to start a conversion.

You can download the SDK for the NHS3152 free of charge from nxp.com: go to www.nxp.com/pages/:NHS3152, click TOOLS & SOFTWARE, scroll down and download SDK 11.2 for NHS3152. Inside, be sure to follow the getting started guide docs/UM_NHS31xx_GettingStarted.pdf, and to check the firmware for an explanation of all the blocks, and code snippets: docs/firmware.html > modules > drivers > i2d: Current to Digital converter driver

This should get you started.

Kind regards,
Dries.

0 项奖励
回复

1,538 次查看
HafizUsman
Contributor I

Hi driesmoors

I am doing one academic assignement where I also have to measre current  using the current sensor of the NHS3152. From the literature and manuals, I came to know that I can take measurements of temperature and other available firmware (HEX files) given as demo. So, I have already downloaded the latest version of SDK12.6.

I think, I have to create a new code (HEX file) using MCUxpresso app for any new activity like current measurement and then I will flash the NHS3152 with this newly developed code (HEX file) using flashmagic app. 

During this activity LPC-lINK2 WILL BE THE MIDDLE PROBE....

please guide me if have conceived the right path and guide about the C++ CODE

Thank you

0 项奖励
回复