NFC tags certification / Regulatory test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC tags certification / Regulatory test

4,229 Views
thomasklatte
Contributor I

What kind of Regulatory Test has to be done for NFC tags? Is a wireless Regulatory Test really required? I like to equip my industrial control with NFC tag chips (passive) for setup and diagnostic. Which standard has to be taken? EN 300330 uses distances  of 3~10m, seems to much for NFC?  And how is the situation for RFID?

0 Kudos
Reply
1 Reply

3,218 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Thomas,

    See following , please!

(1)What kind of Regulatory Test has to be done for NFC tags?

For card, there is some certificate testing, like EMVCo, PBOC etc.

For NFC tag, there is no dedicated universal testing. Some industry customer has their owner company testing .

(2) Is a wireless Regulatory Test really required?

For tag, no.

(3) I like to equip my industrial control with NFC tag chips (passive) for setup and diagnostic. Which standard has to be taken? EN 300330 uses distances of 3~10m, seems to much for NFC?

No need, we have the tag antenna guide, you could take it as the design bench mark. In ISO 14443, has the tag size dimension description.

(4)And how is the situation for RFID?

UHF has the industrial testing standard. Some key projects required this.

Currently there are 2 main certification running. One is ARC test included US and EU band in Auburn University, and the other is TIPP test graded by GS1.

For HF, NO GENERIC ONE, based on the end customer requirement.

Hope above repy can help you !

Best Regards,

Weidong

0 Kudos
Reply