NFC tag with Jcop /smartmx chip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC tag with Jcop /smartmx chip

5,046件の閲覧回数
behdadafghahi
Contributor I

Hi

i am developing application on Jcop smart card using Smart mx chip . just wondering is there any tag to be compatible with this rechnology ?

タグ(1)
0 件の賞賛
返信
2 返答(返信)

4,508件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Behdad Afghahi,

Thank you for using the NFC community.

All JCOP/SmartMX information requests or support inquiries must be directed to your sales representative (FAE or Distributor FAE). If you do not have one already please refer to our distributor network to find a local contact from the next link:

Distributor Network|NXP 

Best Regards!

Jorge Gonzalez

0 件の賞賛
返信

4,503件の閲覧回数
behdadafghahi
Contributor I

Hi

Many thanks , i contact them

but before i came to purchasing phases , i just need to know if there is such tag or not ?

Best Regards

Behdad Afghahi

CEO

VinPaySys AB

Tell # +46 722833730

Adress: Gothia Science Park, Kaplansgatan 16B, no 246, Skövde 541 34 ,Sweden

http://gsp.se/sv/foretagen/vinpaysys

http://www.vinpaysys.com/

0 件の賞賛
返信