NFC reader lib + CLRC66302 in single ended mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NFC reader lib + CLRC66302 in single ended mode

1,077 次查看
ddalfra
Contributor I

Hi All

 

We're working on a LPC1768 and CLRC66302 by using NXP NFCrdlib. So far the porting has gone well.
In our hardware the frontend (CLRC66302) is used in single-ended  and i need to change some register setting, in particular:

 

  1. Rcv register (address 38h)
  2. TxAmp register (address 29h)
  3. TxCon register (address 2Ah)

 

My question is: where's the right place inside NFCrdlib to do that according to the values i need?
I'm working with ISO15693 tags.

 

Thanks in advance

Davide

0 项奖励
回复
0 回复数