NFC device NT3H2111_2211

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC device NT3H2111_2211

ソリューションへジャンプ
4,005件の閲覧回数
andrewbarningha
Contributor III

When i use the NT3H2111 device from fresh i am unable to write to it. I need to format it to NdefFormatable.

I am using the NXP Tag writer App but i do not see anywhere a function to format the device?

Please advise me an App which will allow me to format the device so i can use it.

Thanks

1 解決策
3,853件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear Andrew Barningham,

we recommend to use the NTAG I2C Demoboard - Apps on Google Play   this  application is intended to work with the NTAG i2c and in the configuration tab you can find options to eras, write or read the NTAG i2c.

Please check this and let me know.

BR

Jonathan

元の投稿で解決策を見る

3 返答(返信)
3,854件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear Andrew Barningham,

we recommend to use the NTAG I2C Demoboard - Apps on Google Play   this  application is intended to work with the NTAG i2c and in the configuration tab you can find options to eras, write or read the NTAG i2c.

Please check this and let me know.

BR

Jonathan

3,082件の閲覧回数
nwttyler
Contributor I

What is the current recommended method for formatting this chip for NDEF? I've tried tag writter on IOS and Android with no success and NFC Tools on windows and OSX. The tags are readable, but I cannot write NDEF records to them

0 件の賞賛
返信
3,853件の閲覧回数
andrewbarningha
Contributor III

Thanks, that works.

I used the Reset button to format the device.

0 件の賞賛
返信