NFC Wireless Charging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC Wireless Charging

1,929件の閲覧回数
Shuping
Contributor I
1.What standard this NFC solution applies to? Industrial grade or Consumer grade?
2.Can all NFC excitation magnetic fields be used to charge CRN120? Or must use NXP CTN73X to charge CRN120?
0 件の賞賛
返信
1 返信

1,921件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Shuping ,

 

Please kindly have my comments as below:

1.What standard this NFC solution applies to? Industrial grade or Consumer grade?
- This solution follows the NFC Forum standard, and can be used for Industrial or Consumer applications.
 
2.Can all NFC excitation magnetic fields be used to charge CRN120? Or must use NXP CTN73X to charge CRN120?
-Not all, only the fields meet WLC spec of NFC Forum standard can be used, so better use NXP CTN73X to charge CRN120.
 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信