NFC USB PN533 integration with Android Platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC USB PN533 integration with Android Platform

3,156件の閲覧回数
vinothrajm
Contributor III

Hi ,

   I want to integrate the NFC USB PN533 with Below Platform.

Processor : Mediatek MT6572

OS Platform    : Android - Jelly bean (4.2.2)

Interface   :  USB

Is there any document to integrate NFC USB PN533 in Android platform ?

I get the document for NFC PN544 in below link:

http://www.nxp.com/documents/application_note/AN11690.pdf

NXPNFCLinux · GitHub

Can I use this documents is same as for NFC USB PN533 ?

Please give any guidance to integrate the NFC USB PN533 in Android file system.

Regards,

Vinothraj.

mail: [email protected]

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,559件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Vinothraj,

NXP does not provide PN533 driver on Android. PN544 is a different design from PN533, which is targeted to be applied on Android.


Wish it helps.

Have a great day,
Kan Li
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,559件の閲覧回数
vinothrajm
Contributor III

Hi,

 

Is there anyone have any suggestion for this post. Kindly share me.

Regards,

vinothraj.

0 件の賞賛
返信