NFC Reader and Writer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Reader and Writer

2,886 Views
Fahad
Contributor I

I want to use Mifare Desfire Light or EV2 in a payments product. Given payments, security is paramount including anti-counterfeiting, encryption, MACing, etc. In this regard, I needed confirmation as to whether the NXP Tagwriter app or any other publically available app or tool of NXP can be used to encode/personalize a Desfire chip fulfilling the following security requirements.

 

Key security requirements:

 

Writing/encoding the chip:

  1. Securely writing data on the chip in a manner that the chip is able to authenticate the writer and no other writer can write to the same chip.
  2. Ability to lock the chip so once data is written and chip locked, no one else can write/rewrite/modify data to the same chip.
  3. Ability to write encrypted data on the chip that identifies the customer such as Customer ID, Customer PAN, Expiry date, etc.
  4. Ability to write keys on the chip, which the chip can use to dynamically encrypt data with a unique key for every read from the chip.
  5. Anti-counterfeiting.  
  6. Keys injection/writing on the chip for a Desfire-capable terminal to read/access the chip.

 

Reading the chip:

  1.  The ability of the Desfire-capable terminal to access data through access keys from the chip.
  2. Data so provided by the chip should be dynamically encrypted and with MACing done for authentication on the server.
  3. AES-256 or 128-bit encryption.
  4. Secure messaging from the chip/terminal to the server.  
  5. The server will support verifying MAC sent from the chip and decrypting encrypted data before authorizing the transaction and sending it back to the terminal. There will be no offline transactions. Only online.
  6. The ability of the chip to authenticate a return MAC (optional).

 

Kindly confirm how I can achieve the above with NXP Tagwriter or any other NXP tool in regards to Desfire Light or Desfire EV2 chip.

 

0 Kudos
Reply
3 Replies

2,863 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Fahad ,

 

I would recommend RFIDDiscover full version for that purpose. Please kindly refer to https://www.nxp.com/products/rfid-nfc/mifare-hf/mifare-desfire/rfiddiscover:RFID-DISCOVER for details.

Please note you have to sign a valid NDA with NXP before fetching the full version from NXP doc store.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,758 Views
Fahad
Contributor I

Thanks for your response @Kan_Li .

I want NDA form so, that I can submit accordingly.

0 Kudos
Reply

2,749 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Fahad ,

 

Please kindly follow the steps as shown in https://www.nxp.com/video/tutorial-for-nxp-support-case-portal:NCP-VIDEO to submit the NDA request. The NDA team would contact you later for further assistance.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply