NFC - Not allowed numbers in Tag ID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC - Not allowed numbers in Tag ID

1,763 Views
fernandohcoelho
Contributor III

Hi everyone, I have a doubt about tag id numbers.

I found in some documentation that the hexadecimals 81h to FEh should never be used in the "manufacturer identification" - first byte of tag id. For NXP, it will be 04h.

We are reading NXP NTAG213 and sending information through serial RS232, using separators like pipe. Altought it worked fine so far, we are affraid at some point the hexadecimal representation of this char (7Ch in case of pipe) will appear middle of Tag Id, causing an error.

So, the question is: Is there any hexadecimal that would never appear in a Tag Id? 

Thanks!!!

Fernando Coelho

Tags (2)
0 Kudos
Reply
1 Reply

1,637 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Fernando,

Would you please specify which documentation mentions this information?

Thanks for your patience!


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply