NFC License Requirements

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC License Requirements

2,012件の閲覧回数
scarey-css
Contributor I

I am trying to identify what (if any) license requirements there are when using the PN7462 family, PN7150, or CLRC663 family as card readers and/or peer-to-peer devices. In the datasheet for each device it explicitly lists in the license section that the device comes with the right for use with ISO/IEC 14443 Type B software under Innovation's Contactless Card patents license. But it does NOT list ISO/IEC 14443 Type A in the licenses section. Does this fall under a separate license? If so, where can I get more information about this?

Similarly, the licenses section explicitly states that the ISO/IEC 18092 and 21481 are not licensed by this product. What licenses are required for those standards and where can I find more information about them?

0 件の賞賛
返信
1 返信

1,977件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @scarey-css ,

 

For non-technical issues, please contact your local NXP sales representatives for further support.

 

Thanks for your patience and understanding!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信