NFC Forum type 4A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC Forum type 4A

2,736件の閲覧回数
andrewbarningha
Contributor III

Please can anyone advise me what devices NXP do which support NFC Forum type 4A with I2C interface.

I have been using the NT3H1101 device but need to use the forum type 4A.

Thanks

2 返答(返信)

2,580件の閲覧回数
manojrohitvempa
Contributor II

Hello,

You can use NFC-explore which has Pn512 nfc Transponder. The NFC Reader library can be used as the Software which has both SPI and I2C Interface.

The demo explore-nfc Basic uses SPI Interface.

2,580件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

I am sorry, but so far we just have NFC Forum type 4A tag without I2C interface.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------