NFC Electromagnetic Compatibility for CE compliance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Electromagnetic Compatibility for CE compliance

3,174 Views
fourtrax
Contributor I

Hi, I am using a PN532 and experiencing the problem that energy is magnetically coupled from the NFC antenna into the power cords that are connected to my device.

I did a precompliance measurement using a spectrum analyser and a DC-LISN that shows values above the 1mV limit for 13.56 Mhz (no harmonics or anything else).

Unfortunately I can not move the connector further away from the antenna on the pcb, also attempts to shield it using a ferrite sheet didn't help much. Twisting the power cable reduces the peak but I can not rely on that being done by the user.

Will the 13.56 Mhz peak make me fail the EMC conducted emission test or are there any exceptions for NFC regarding conducted (and radiated) emissions ?

thanks in advance

0 Kudos
Reply
1 Reply

2,904 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Gerrit,

   About CE certification of PN532, you can contact mobile team of local NXP.

Best regards,

Weidong Sun

0 Kudos
Reply