NFC Cockpit not seeing OM25180FDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Cockpit not seeing OM25180FDK

1,984 Views
KevinBraun
Contributor I

Hello,

I have a brand new NFC Cockpit setup on a Windows 10 machine.  After a few struggles, I now have the USB COM port set up properly, NxpNfcCockpit VCOM (COM5). 

I installed NFC Cockpit on my D: drive,  D:\nxp\NxpNfcCockpit_v4.8.0.0\bin\NxpNfcCockpitGUI.exe

NFC Cockpit does not see the OM25180 board. Open Port, Soft Reset, etc. are greyed out and the Log Monitor shows nothing.

The board has a blue(PN_RST), green(IRQ), dull red(LD100) LED on and a flashing orange(LD200) LED

Thanks,

...kevin

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,800 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

It would be helpful to refer to chapter 3 of AN11744 regarding the necessary firmware for PN5180.

Hope this helps.

Have a nice day,

Ivan.

0 Kudos
Reply