NFC Cockpit cannot detect board PNEV5190B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Cockpit cannot detect board PNEV5190B

3,768 Views
mbougouin
Contributor I

Hello,

I am trying to connect to my PNEV5190B Board, but NFC Cockpit doesn't seem to work.

The board is plugged on my laptop via an USB cable, and the board is powered up. When pressing the refresh button, software doesn't react.

NCF Cockpit's log seemed to indicate a problem with ADB process :

[2024.06.07 13:23:21]:DEBUG :ServiceBroker :MainWindow registration successfull
[2024.06.07 13:23:21]:DEBUG :ServiceBroker :ReadWriteNotify registration successfull
[2024.06.07 13:23:21]:WARN :OnlineVersionCheck :Please check your Internet connection!
[2024.06.07 13:23:23]:DEBUG :BoardDetect :Unable to load ADB process. Check if adb is part of environment variable
[2024.06.07 13:23:23]:DEBUG :BoardDetect :Exception details:
[2024.06.07 13:23:23]:DEBUG :BoardDetect : Type : System.ComponentModel.Win32Exception
[2024.06.07 13:23:23]:DEBUG :BoardDetect : Message: Le fichier spécifié est introuvable

VCOM files have been installed.

I changed USB cable.

0 Kudos
Reply
3 Replies

3,748 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @mbougouin 

Please update NFC Cockpit fw, the attached for your reference.

0 Kudos
Reply

3,700 Views
mbougouin
Contributor I

Hello @KaiLi,

I am not sure that your answer is relevant.

It's NFC cockpit that's not detecting the connected board.

 

I can repeat my problem, with PNEV5190B board connected or not, the result is the same.

So I don't know why updating the board firmware will help me...

 

0 Kudos
Reply

3,693 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @mbougouin 

What I mean is that you need to update the firmware of the board to NFC Cockpit as shown below, there is no VCOM port available from your log. Have you updated the bin file below?

KellyLi_0-1718014463587.png

 

0 Kudos
Reply