MFRC522 and RC522 Consultation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFRC522 and RC522 Consultation

4,903件の閲覧回数
Karyliu
Contributor II

Hi NXP,

What's the main difference between MFRC522 and RC522?

Do these two chips support use on the operating system (Windows \ Android \ Linux)? Is there a corresponding driver code?

Are there any restrictions on the main control chips that these two ICs can be paired with?

What support does NXP provide for these two chips?

Thank you.

0 件の賞賛
返信
5 返答(返信)

4,860件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Karyliu 

What's the main difference between MFRC522 and RC522?
Ans: Actually, the two are the same product.

Do these two chips support use on the operating system (Windows \ Android \ Linux)? Is there a corresponding driver code?
Ans: Just running on Windows, and there are not any examples for reference.

Are there any restrictions on the main control chips that these two ICs can be paired with?
Ans: No restrictions, just SPI interface communication should be available.

What support does NXP provide for these two chips?
Ans: As the MFRC522 is not recommended for new designs we do not have more information but the one in the public we page. We have some examples for some LPC's and other Kinetis files for the recommended products CLRC663 plus.

 

Best Regards,

kelly

0 件の賞賛
返信

4,845件の閲覧回数
Karyliu
Contributor II

Hi Kelly,

Thank you for your reply!

Does CLRC663 support freeRTOS?

Is there any restriction on MCU.

Thank you.

0 件の賞賛
返信

4,834件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Karyliu 

Yes, CLRC663+MCU can run with FreeRTOS, and NXP provides the examples all based on FreeRTOS.

For MCU, which is no limitation, just has SPI or I2C interface should be ok.

Best Regards,

kelly

0 件の賞賛
返信

4,829件の閲覧回数
Karyliu
Contributor II

Hi Kelly,

Are there any restrictions on MCU manufacturers/models?

Thank you.
0 件の賞賛
返信

4,822件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Karyliu 

It's best to choose NXP MCUS because NXP offers routines that are based NXP's MCUS, such as LPC1769 and FRDM-K82F for your reference.

Best Regards,

kelly

0 件の賞賛
返信