MFRC522 - TX1 and TX2 Impedance Matching

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MFRC522 - TX1 and TX2 Impedance Matching

2,522 次查看
spanda
Contributor I

Hi guys,

I am designing a RFID Module using MFRC522 chip. So while designing the layout of the board, I wanted to confirm the impedance matching to be performed on TX1 and Tx2 lines . I want my Rmatch to be 50 Ohms. Then do I need both TX1 and Tx2 traces to be 50 Ohms single endedly or should the differential impedance between them be 50 ? I think it is differential but still I would like it confirmed.

Best,

Soumya

标记 (2)
0 项奖励
回复
1 回复

2,389 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

As mentioned in the case, the matching has to be done for the antenna values, and  the distances between components in the matching circuit shall be as short as possible.

Regards,

Ivan.

0 项奖励
回复