Hi,
in the nhs3100 SDK file lib_chip_nss/inc/nfc_nss.h is a reference to 3 examples. Here is corresponding nfc_nss_example_1.c example:
* @par Example 1 - Simple NDEF Message Write
* The below example demonstrates how a simple NDEF message can be written to the shared memory which can then be read
* by an external reader. Refer to @ref MODS_NSS_NDEFT2T for a simplified API to handle NDEF Messages.
* @snippet nfc_nss_example_1.c nfc_nss_example_1
How can I download this example? It seems to be not in the SDK.
BR
Hi,
In the NHS3100 SDK 11.2: open docs/firmware.html, then from the left pane navigate to Modules > Modules > ndeft2t. The right pane now shows the full ndeft2t documentation, including the example code snippets:
Example1 - Creating an NDEF Message with a single record of type TEXT
NDEF messages consisting of a single record of types MIME, AAR and URI can be created in a similar way as given in this example.
uint8_t instanceBuffer[NDEFT2T_INSTANCE_SIZE] __attribute__((aligned (4)));uint8_t messageBuffer[NFC_SHARED_MEM_BYTE_SIZE ] __attribute__((aligned (4)));NDEFT2T_CREATE_RECORD_INFO_T createRecordInfo;uint8_t locale[] = "en";uint8_t payloadText[] = "Hello World";/* Ensure initialization of the NFC HW block is done first. This needs to be done only once.* Any previously written NDEF message will be lost as the NFC shared memory will be re-initialized.*/NDEFT2T_Init(); /* Required once, not for every message creation or parsing. */createRecordInfo.shortRecord = 1; /* Enable Short record */createRecordInfo.pString = locale;/* The payload length to pass excludes the NUL terminator. */NDEFT2T_CommitRecord((void*)instanceBuffer);}}NDEFT2T_CommitMessage((void*)instanceBuffer);/* The return value of the commit function is ignored here. However, the application should use it appropriately. */
Best,
Dries.